Controls point-to-point smoothing. Smoothing is a noise reduction technique that averages adjacent data points in a measurement trace. Choose the amount of smoothing by specifying either the number of points or the aperture. Smoothing is not the same as CALC:AVERage which averages each data point over a number of sweeps.
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
|
(Read-Write) Sets the amount of smoothing as a percentage of the number of data points in the channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<num> |
Percentage value. Choose any number between: |
|
Examples |
CALC:SMO:APER 2 calculate2:smoothing:aperture 20.7 |
|
Query Syntax |
CALCulate<cnum>:SMOothing:APERture? |
|
Return Type |
Numeric |
|
1.5 |
|
|
(Read-Write) Sets the number of adjacent data points to average. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<num> |
Number of points from 1 point to maximum of 25% of data points in the channel. For example: if number of points in a data trace = 401, the maximum value for points = 100. The points value is always rounded to the closest odd number. |
|
Examples |
CALC:SMO:POIN 50 calculate2:smoothing:points 21 |
|
Query Syntax |
CALCulate<cnum>:SMOothing:POINts? |
|
Return Type |
Numeric |
|
3 |
|
|
(Read-Write) Turns data smoothing ON or OFF. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<ON | OFF> |
ON (or 1) - turns smoothing ON. |
|
Examples |
CALC:SMO ON calculate2:smoothing:state off |
|
Query Syntax |
CALCulate<cnum>:SMOothing[:STATe]? |
|
Return Type |
Boolean (1 = ON, 0 = OFF) |
|
OFF |
|