This example program does the following:
Create an iTMSA Balanced Sdd21 measurement
Set sweep type = power
Set phase offset on balanced port 1=180 degrees
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as Balanced.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
|
Dim app Dim scpi ' Create / Get the PNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser ' Reset the system scpi.Parse("SYST:FPRESET") ' This example uses DUT topology Bal-Bal - ' Turn on a window scpi.Parse("DISP:WIND1:STATe ON") ' Create a trace called "sdd21", and for that trace turn on the balanced ' transformation and set the balanced transformation to BBAL SDD21. scpi.Parse("CALC:PAR:DEF:EXT ""sdd21"",S11") ' Feed the sdd21 trace to window 1, trace 1 scpi.Parse("DISP:WIND1:TRAC1:FEED ""sdd21""") scpi.Parse("CALC:PAR:SEL ""sdd21""") ' Set the topology of measurement scpi.Parse("CALC:FSIM:BAL:DEVice BBALanced") scpi.Parse("CALC:FSIM:BAL:TOPology:BBAL:PPORts 1,3,2,4") ' Set up stimulus scpi.Parse("SENS:SWE:POINts 801") scpi.Parse("SENS:FREQ:STARt 10e6") scpi.Parse("SENS:FREQ:STOP 1e9") scpi.Parse("CALC:FSIM:BAL:PAR:STATe ON") scpi.Parse("CALC:FSIM:BAL:PAR:BBAL:DEF SDD21") ' Recall a 4-port Cal Set or perform a 4-port Cal here
' Set the sweep type to power sweep scpi.Parse("SENS:SWE:TYPE POWer") ' Set iTMSA parameters scpi.Parse("CALC:FSIM:BAL:BPOR1:OFFS:PHAS 180") scpi.Parse("CALC:FSIM:BAL:FIXT:OFFS:PHAS ON") scpi.Parse("CALC:FSIM:BAL:STIM:MODE TM")
|