This VBScript file performs a 2-Port Guided TRL calibration on 2-port PNA analyzers. (See an example of TRL cal on a 4-port PNA.) This program does the following:
Clear old measurements from the PNA
Create a new S22 measurement
Set an instrument state
Select the connectors and cal kit
Initiate a Guided calibration
Display a prompt as each new standard must be connected
Save the calibration to a newly created cal set.
Note: This program runs without error on all PNA code revisions 7.21 and higher.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as TRL.vbs. Learn how to setup and run the macro.
|
Dim App Dim Parser Dim Chan Dim txtDat Dim step Dim parserTxt Dim prompt Set App = CreateObject("AgilentPNA835x.Application") ' Clear old measurements App.Reset ' Create a new Measurement Set Parser = App.SCPIStringParser Parser.Parse "DISPlay:WINDow1:STATE ON" Parser.Parse "CALCulate:PARameter:DEFine:EXT 'MyMeas',S12" Parser.Parse "DISPlay:WINDow1:TRACe1:FEED 'MyMeas'" ' Initialize state Set Chan = App.ActiveChannel Chan.StartFrequency = 18.0e9 Chan.StopFrequency = 20.0e9 Chan.IFBandwidth = 1000 ' Begin a guided calibrations Parser.Parse "SENS:CORR:COLL:GUID:CONN:PORT1 'APC 3.5 male'" Parser.Parse "SENS:CORR:COLL:GUID:CONN:PORT2 'APC 3.5 female'" Parser.Parse "SENS:CORR:COLL:GUID:CKIT:PORT1 '85052C'" Parser.Parse "SENS:CORR:COLL:GUID:CKIT:PORT2 '85052C'" ' Select TRL cal method. Parser.Parse "SENS:CORR:COLL:GUID:PATH:CMET 1,2,'TRL'" txtDat = Parser.Parse("SENS:CORR:COLL:GUID:PATH:CMET? 1,2") MsgBox("Method " + txtDat) Parser.Parse "SENS:CORR:COLL:GUID:INIT" ' Query the number of steps txtDat = Parser.Parse("SENS:CORR:COLL:GUID:STEP?") ' Display the number of steps MsgBox("Number of steps is " + txtDat) ' Set the loop counter limit step = CInt(txtDat) ' Measure the standards For i = 1 To step parserTxt = "sens:corr:coll:guid:desc? " + CStr(i) prompt = Parser.Parse(parserTxt) MsgBox(prompt) parserTxt = "sens:corr:coll:guid:acq STAN" + CStr(i) Parser.Parse (parserTxt) Next ' All standards have been measured. Save the result Parser.Parse "SENS:CORR:COLL:GUID:SAVE" MsgBox("The TRL calibration has been completed") |