This example program performs Thru Response cals in both the forward and reverse directions. It does this by selecting the appropriate measurement right before acquiring the standard. The cal infers the direction from the measurement.
This program also demonstrates the use of the SENSe:CORR:PREF:CSET:SAVE command. The details are in the comments.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as Unguided.vbs. Learn how to setup and run the macro.
|
Dim App Set App = CreateObject("AgilentPNA835x.Application") Dim Parser Set Parser = App.SCPIStringParser 'Preset and delete measurement Parser.Parse "SYSTem:FPReset" 'The following commands determine how the cal set is saved. 'Pick one of the following preferences, comment the other 'Save cals to separate new USER CalSets 'Parser.Parse "SENS:CORR:PREF:CSET:SAVE USER" 'Save both cals to a single cal register 'Parser.Parse "SENS:CORR:PREF:CSET:SAVE CALR" 'Save both cals to a single currently selected CalSet or register Parser.Parse "SENS:CORR:PREF:CSET:SAVE REUSE" ' 'Create a new S21 Measurement Parser.Parse "CALCulate:PARameter:DEFine:EXT 'MyS21Meas',S21" Parser.Parse "DISPlay:WINDow1 ON" Parser.Parse "DISPlay:WINDow1:TRACe1:FEED 'MyS21Meas'" 'Create a new S12 Measurement Parser.Parse "CALCulate:PARameter:DEFine:EXT 'MyS12Meas',S12" Parser.Parse "DISPlay:WINDow1:TRACe2:FEED 'MyS12Meas'" 'Turn off continuous sweep Parser.Parse "INITiate:CONTinuous OFF" 'Begin cals 'Select a cal kit Parser.Parse "SENSe:CORRection:COLLect:CKIT:SELect 1" 'Perform a forward thru response cal 'Select the S21 Meas Parser.Parse "CALCulate1:PARameter:SELect 'MyS21Meas'" 'Set the calibration method to Thru Response Parser.Parse "SENSe1:CORRection:COLLect:METHod TRAN1" MsgBox("Connect Thru between ports Then press OK") Parser.Parse "SENSe1:CORRection:COLLect:ACQuire STAN4" Parser.Parse "SENSe1:CORRection:COLLect:SAVE" 'Then perform a reverse thru response cal 'Change measurement to S12 Parser.Parse "CALCulate1:PARameter:SELect 'MyS12Meas'" 'Set the calibration method to Thru Response Parser.Parse "SENSe1:CORRection:COLLect:METHod TRAN1" 'Ensure the thru connection is still in place 'Acquire Thru std in reverse direction Parser.Parse "SENSe1:CORRection:COLLect:ACQuire STAN4" 'All standards have been measured. Parser.Parse "SENSe1:CORRection:COLLect:SAVE" 'Turn ON continuous sweep Parser.Parse "INITiate:CONTinuous ON" MsgBox("The calibration has been completed") |