This example performs a Guided Calibration using TWO power sensors that are setup as PMAR devices. Use of two power sensors is necessary when the frequency range of the measurement is greater than can be attained with a single sensor.
A measurement must first be set up with desired frequency range, power, and so forth, ready to be calibrated.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do not need to control the PNA via GPIB to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the PNA hard drive as mps.vbs.
Learn how to setup and run the macro.
See Guided Power Sensor SCPI commands
See Other SCPI Example Programs
set app = CreateObject("Agilentpna835x.application") set s = app.ScpiStringParser s.Parse "SYST:PRES" s.Parse "SENS:FREQ:START 1E9" s.parse "SENS:FREQ:STOP 2E9" s.Parse "sens:corr:coll:guid:conn:port1 'APC 3.5 female'" s.Parse "sens:corr:coll:guid:conn:port2 'APC 3.5 male'" s.Parse "sens:corr:coll:guid:ckit:port1 'N4691-60004 ECal'" s.Parse "sens:corr:coll:guid:ckit:port2 'N4691-60004 ECal'" s.Parse "SENS:CORR:COLL:GUID:PSEN2 ON" 'turn on power cal at port #2 s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT ON" s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT:NAME 'pmar1'" s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT:FREQ:STARt 1e9" s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT:FREQ:STOP 1.5e9" s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT:ADD 'PMAR2'" s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT2:FREQ:STARt 1.5e9" s.Parse "SENS:CORR:COLL:GUID:PSEN2:MULT2:FREQ:STOP 2e9" s.Parse "SENS:CORR:COLL:GUID:INIT" numSteps = s.Parse("SENS:CORR:COLL:GUID:STEPS?") for i = 0 to numSteps-1 desc = s.parse("SENS:CORR:COLL:GUID:DESC? " & CStr(i+1)) msgbox desc s.parse "SENS:CORR:COLL:GUID:ACQ STAN" & CStr(i+1) next s.parse "SENS:CORR:COLL:GUID:SAVE" |