This example program does the following:
Sets up measurement for either PNOP or PSAT marker search
Sets parameters for search
Reads a parameter for each
See PNOP and PSAT SCPI commands.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as SearchMkr.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
|
Dim app Set app = CreateObject("AgilentPNA835X.Application") Dim scpi set scpi = app.ScpiStringParser scpi.Execute ("SYST:FPReset") ' View Power Out vs Power In ' Create and turn on window/channel 1 scpi.Execute ("DISPlay:WINDow1:STATE ON") 'Define a measurement name, parameter scpi.Execute ("CALCulate1:PARameter:DEFine:EXT 'MyMeas',B") 'Associate ("FEED") the measurement name ('MyMeas') to WINDow (1) scpi.Execute ("DISPlay:WINDow1:TRACe1:FEED 'MyMeas'") scpi.Execute ("CALCulate1:PARameter:SELect 'MyMeas'") 'perform power sweep scpi.Execute ("SENSe1:SWEep:TYPE POWer") scpi.Execute ("SOURce1:POWer:STARt -5") scpi.Execute ("SOURce1:POWer:STOP 0") '-------------------- 'Choose marker search resp=Msgbox ("PNOP (yes) or PSAT (no)" , 4, "PNA Marker Search Demo") if resp=6 then PNOP1() Else PSAT1() End If '-------------------- 'PSAT marker search Sub PSAT1() scpi.Execute ("CALCulate1:MARKer:PSATuration:BACKoff 2") 'Read PSAT Parameter dim answer answer=scpi.Execute ("CALCulate1:MARKer:PSATuration:GAIN?") wscript.echo("Gain Sat: "& answer) End Sub '-------------------- 'PNOP marker search Sub PNOP1() scpi.Execute ("CALCulate1:MARKer:PNOP:BACKoff 2") scpi.Execute ("CALCulate1:MARKer:PNOP:POFFset 1") 'Read PNOP Parameter dim answer answer=scpi.Execute ("CALCulate1:MARKer:PNOP:GAIN?") wscript.echo("PNOP Gain: "& answer) End Sub |