Initiates a Power Normal Operating Point marker search and reads the results.
CALCulate:MARKer:PNOP | GAIN? | PIN? | POUT? | MAXimum? | MAXimum? | MAXimum? | MAXimum? |
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
(Read-Write) Turns on and sets markers 1, 2, 3, and 4 to calculate various PNOP parameters. Either this command, or the POFFset command, will initiate the PNOP search markers. To turn off the PNOP markers, either turn them off individually or turn them All Off. To search a User Range with the PNOP search, first activate marker 1 and set the desired User Range. Then send CALC:MARK:PNOP:BACK. The user range used with the PNOP search only applies to marker 1 searching for the linear gain value. The other markers may fall outside the user range. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<num> |
Backoff value. Choose any number between :-500 and 500 |
Examples |
CALC:MARK:PNOP:BACK? calculate2:marker:pnop:backoff 10 |
Query Syntax |
CALCulate<cnum>:MARKer:PNOP:BACKoff? |
Return Type |
Numeric |
|
|
(Read-only) Reads the power backoff gain value from a PNOP marker search. PBO Gain = PBO Out - PBO In Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:BACK:GAIN? |
Not applicable |
|
(Read-only) Reads the power backoff input value from a PNOP marker search. PBO In = Marker 2 X-axis Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:BACK:PIN? |
Not applicable |
|
(Read-only) Reads the power backoff output value from a PNOP marker search. PBO Out = Marker 2 Y-axis Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:BACK:POUT? |
Not applicable |
|
(Read-only) Reads the PNOP compression value from a PNOP marker search. Pnop Comp = Pnop Gain - Linear Gain (not shown on marker readout). Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:COMP? |
Not applicable |
|
(Read-only) Reads the max compression value from a PNOP marker search. Comp Max = Gain Max - Linear Gain (not shown on marker readout). Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:COMP:MAX? |
Not applicable |
|
(Read-only) Reads the PNOP gain value from a PNOP marker search. Pnop Gain = Pnop Out - Pnop In. Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:GAIN? |
Not applicable |
|
(Read-only) Reads the max gain from a PNOP marker search. Gain Max = PMax Out - PMax In Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:GAIN:MAX? |
Not applicable |
|
(Read-only) Reads the PNOP input value from a PNOP marker search. Pnop In = Marker 4 X-axis value Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:PIN? |
Not applicable |
|
(Read-only) Reads the max input power from a PNOP marker search. PMax In = Marker 3 X-axis value Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:PIN:MAX? |
Not applicable |
|
(Read-Write) Turns on and sets markers 1, 2, 3, and 4 to calculate various PNOP parameters. Either this command, or the Backoff command, will initiate the PNOP search markers. To turn off the PNOP markers, either turn them off individually or turn them All Off. To search a User Range with the PNOP search, first activate marker 1 and set the desired User Range. Then send the CALC:MARK:PNOP:POFF command. The user range used with the PNOP search only applies to marker 1 searching for the linear gain value. The other markers may fall outside the user range. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<num> |
Power Offset value in dB. Choose any number between :-500 and 500 |
Examples |
CALC:MARK:PNOP:POFF 3 calculate2:marker:pnop:poffset 10 |
Query Syntax |
CALCulate<cnum>:MARKer:PNOP:POFFset? |
Return Type |
Numeric |
|
|
(Read-only) Reads the output power value of the offset marker from a PNOP marker search. Pnop Out = Marker 4 Y-axis value Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:POUT? |
Not applicable |
|
(Read-only) Reads the max output power from a PNOP marker search. PMax Out = Marker 3 Y-axis value Use CALC:MARK:PNOP:BACK or CALC:MARK:PNOP:POFF to initiate a PNOP search. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:MARK:PNOP:POUT:MAX? |
Not applicable |
|