In this topic:
Beginning in Sept. 2013, the PNA is shipped from the factory with Windows® Embedded Standard 7 operating system. This OS supports both 32-bit and 64-bit applications. Therefore, the file structure has changed slightly. ONLY PNA models with Windows 7 can upgrade to FW A.10.00 and above. Learn about Windows 7 file locations on the PNA.
The leading cause of PNA failures is problems with the PNA Hard Disk Drive (HDD). These problems are usually preventable, and in many cases, recoverable. Learn more about protecting your PNA.
The PNA has USB ports on the front panel and on the rear panel. The main advantages of USB are “hot” connects and disconnects and fast data transfer speeds. Electronic Calibration modules are also available with USB connections.
The first time you plug a device into a USB port there is some wait time. Windows reports it is identifying the hardware, then searching for the correct driver, then installing the driver (if it was found).
Connecting that same device back into that same port later is quick and easy, but if you move the device to a different USB port, you will have to wait through the hardware ID and driver search again.
Windows supports DHCP and fixed IP addressing. Also, “Hot” connect and disconnect of the LAN cable, as well as a visual indicator of LAN status in system tray area, makes LAN connections more intuitive. In addition, the Hardware Wizard helps users with system hardware configuration.
Single and Double Click option
By default, Windows allows a single-click method of launching icons. To revert to double-clicking, click Start, then Settings, then Control Panel, then click Mouse. In the Mouse Properties dialog, select Double-click to open an item. Then click OK.
The PNA application is designed for, and best viewed in, Keysight Technologies theme. To change the theme:
Right-click on the Desktop, then click Personalize
Use the scrollbar, then select a Theme.
Adding a printer should be done outside of the PNA application. Learn more.
Last modified:
|
25-Nov-2013 |
Modified for Windows 7 |