Other topics about Advanced Mode
The following table shows the comparison of Advanced and Basic Modes.
|
Mode |
Feature |
TDR Application (User Interface) |
Hard Key on Front Panel |
Soft Keys (right side of the screen) |
Measurement Class Selection |
Indicators |
|
Advanced1 |
|
Available |
Available |
Available |
Available but not recommended |
TDR indicator + SVC indicator |
|
Basic |
Easy to use |
Available |
Locked except for Trace Prev, Trace Next, Trace Max and keys in numeric key pad. |
Hidden |
Not Available |
1 Setting VNA-TDR to Advanced Mode enables VNA functions which are disabled in Basic Mode. It is possible to set up features that will result in unexpected measurement results. Therefore, only advanced users should use Advanced Mode.
The sample measurements are shown in the measurement examples.
In the Advanced Mode, you can access all VNA functions. The setting you changed may affect the measurement unexpectedly. The measurement may not be correct if you have such a case. Therefore, the measurement performance is not guaranteed in the Advanced Mode.
It is known that changing the following settings can cause incorrect measurement.
|
Hard key |
Do not use |
|
Meas |
Single end 1 port: Parameters related with ports 2, 3 and 4 |
|
Trace |
Add / Delete Traces |
|
Display |
Data Math, Equation Editor |
|
Sweep Setup |
Start/Stop/Center/Span Points Sweep Type Frequency Offset |
|
Calibration |
Fixture Simulator, AFR (If you want to use AFR, create a snp file in standard class, then use the embedding in adv waveform) |
|
Marker Function |
Marker -> Start, Marker -> Stop |
Here is another caution in the Advanced Mode.
|
Function |
Note |
|
|
Meas |
Change parameter when Port extension on |
This may cause to tilt the wave form in the time domain . Use TDR GUI to select parameter. |
|
Display |
Increasing Num of Trace |
This may cause to tilt the wave form in the time domain. |
|
Analysis |
Fixture Simulator |
This may cause to tilt the wave form in the time domain. |
|
Transform > Window > Impulse width or Step Rise |
The range of these settings is narrower than one of the Rise Time in the TDR GUI. Use TDR GUI to set the rise time. |
|
|
Calibration |
Increasing Port Extension |
This may cause to exceed the DUT length limitation. |
|
Scale |
Increasing Electrical Delay |
This may cause to exceed the DUT length limitation. |
|
Ave |
IF Bandwidth |
Even if you have narrow IF Bandwidth, you may not have noise reduction at lower frequency. |