Broadband System Measurement Setup

Broadband refers to mmWave configurations with a frequency range of 900 Hz to 110 GHz (N5290A) or 900 Hz to 120 GHz (N5291A). This configuration spans the entire frequency range in a single sweep.

After minimal setup shown below, the N5290A/91A functions the same as a standard VNA. All ports can be used at mmWave frequencies or a combination as required.

In this topic:

Limitations

See Also

Setting Up a Measurement

  1. Press Setup > External Hardware > Millimeter Config.
  2. Select N5291A Broadband (or N5290A Broadband).

  1. Note the ports selected for Enable Modules. Frequency Extenders connected to the test set are automatically detected. Configure as necessary.
  2. Press OK. This closes the dialog.
  3. To change the start frequency below 10 MHz (minimum of 900 Hz), press Freq > Main > Start then enter the start frequency below 10 MHz. The following dialog is displayed.

  1. Click OK.
  2. To change the stop frequency, press Freq > Main > Stop then enter the stop frequency.