Write-only
About Auto Port Extensions

AutoPortExtReset Method


Description

Clears old port extension delay and loss data in preparation for acquiring new data. Send this command prior to sending a new series of measurements using AutoPortExtMeasure Method. If acquiring both OPEN and SHORT standards, do not send this command between those acquisitions.

 VB Syntax

fixture.AutoPortExtReset

Variable

(Type) - Description

fixture

A Fixturing (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

fixture.AutoPortExtReset

C++ Syntax

HRESULT AutoPortExtReset();

Interface

IFixturing2