Read
About Receiver Leveling

RangeGetMinPower Method


Description

Returns the maximum of all minimum power values from RangeStartFrequency to RangeStopFrequency (inclusive).

 VB Syntax

minPower = powerRange.RangeGetMinPower

Variable

(Type) - Description

powerRange

A PowerRange (object)

minPower

(Double) Variable to store the power level in dBm.

Return Type

(Double)

Default

Not Applicable

minPower = powerRange.RangeGetMinPower

C++ Syntax

HRESULT get_RangeGetMinPower(double* pMin);

Interface

IPowreRange