MeasurementClassProperties Object


Description

These properties return properties of specific measurement classes.

Accessing the MeasurementClassProperties object

Set app = CreateObject("AgilentPNA835x.Application")

Set cap = app.Capabilities

'Access the MeasurmentClassProperties Object

Set measProps = cap.MeasurmentClassProperties ("Swept IMD")

list=measProps.SupportedParameters

See Also

Methods

Interface

See History

 

None

 

 

Properties

 

Description

SupportedParameters

MeasurementClassProperties

 

IMeasurementClassProperties History

Interface

Introduced with VNA Rev:

IMeasurementClassProperties

9.40