Read only
About Measurement Classes

MeasurementClassProperties Property


Description

Provides access to the MeasurementClassProperties Object.

 VB Syntax

handle = cap.MeasurementClassProperties (measClass)

Variable

(Type) - Description

handle

(Variant) - Variable to store the returned object.

cap

A Capabilities (object)

measClass

(String) Name of the measurement class to be accessed.

Use AvailableMeasurementClasses Property to return a list of measurement classes installed on the VNA.

Return Type

Object

Default

Not Applicable

Examples

'Access the MeasurmentClassProperties Object

Set app = CreateObject("AgilentPNA835x.Application")

Set cap = app.Capabilities

Set measProps = cap.MeasurmentClassProperties("SweptIMD")

C++ Syntax

HRESULT put_MeasurementClassProperties(IMeasurementClassProperties *handle);

Interface

ICapabilities8