A collection object that provides a mechanism for iterating through the segments of the power loss table used with a Power Meter as Receiver. The power loss table can contain up to 9999 segments.
Example: Create a PMAR Device and Measurement
Methods |
Description |
---|---|
Adds a PowerLossSegmentPMAR object to the collection. |
|
Use to get a handle to a PowerLossSegmentPMAR object in the collection. |
|
Removes a PowerLossSegmentPMAR object from the collection. |
|
Properties |
Description |
Returns the number of PowerLossSegmentPMAR objects in the collection. |
|
Returns a handle to the Parent object of this collection. |
Interface |
Introduced with PNA Rev: |
IPowerLossSegments |
9.0 |