The following program creates a new External Device: a Power Meter as Receiver, makes several power meter settings, and then creates a PMAR measurement.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as PMAR.vbs. Learn how to setup and run the macro.
PowerSensorCalFactorSegmentPMAR Object
PowerLossSegmentsPMAR_Collection
| 
 dim app Set app = CreateObject("AgilentPNA835x.Application") dim externalDevices Set externalDevices = app.ExternalDevices dim devicecount devicecount = externalDevices.count externalDevices.Add "NewPMAR" dim newExternalDevice Set newExternalDevice = externalDevices.Item("NewPMAR") newExternalDevice.DeviceType = "Power Meter" newExternalDevice.IOConfiguration= "GPIB0::14::INSTR" 'newExternalDevice.IOConfiguration = "USB0::2391::4865::GB45100278::0::INSTR" newExternalDevice.IOEnable = true dim PMAR Set PMAR = newExternalDevice.ExtendedProperties PMAR.SensorIndex = 1 PMAR.ReadingsPerPoint = 10 dim avr avr = PMAR.ReadingsPerPoint PMAR.ReadingsTolerance = 0.1 dim tole tole = PMAR.ReadingsTolerance PMAR.MinimumFrequency = 100000000 PMAR.MaximumFrequency = 10000000000 PMAR.LimitFrequency = false PMAR.referenceCalFactor = 99 Set powerCalFactorSegments = PMAR.CalFactorSegments powerCalFactorSegments.Add 1,10 Set calpair = powerCalFactorSegments(1) calpair.Frequency = 1e9 calpair.CalFactor = 99 Set calpair = powerCalFactorSegments(2) calpair.Frequency = 2e9 calpair.CalFactor = 98 powerCalFactorSegments.Remove 3,8 PMAR.UsePowerLossSegments = true Set pls = PMAR.PowerLossSegments pls.Add 1,5 Set pl = pls(1) pl.Loss = -1 pl.Frequency = 1e9 Set pl = pls(2) pl.Loss = -2 pl.Frequency = 2e9 pls.Remove 3,3 newExternalDevice.active = true 'Create a PMAR trace with power meter connected to port 3 app.CreateMeasurement 1,"NewPMAR",3,1 
  |