PowerSensorCalFactorSegmentPMAR Object


Description

Contains the properties describing a segment of a power sensor cal factor table that is used with Power Meter as Receiver.

Accessing the PowerSensorCalFactorSegment PMAR object

You can get a handle to one of these segments through CalFactorSegmentsPMAR.Item(n).

See Also

Methods

 

None

 

Properties

Description

Frequency

The frequency (Hz) associated with this segment.

CalFactor

The cal factor (%) associated with this segment.

SegmentNumber

Returns the number of this segment.

 

IPowerSensorCalFactorSegment History

Interface

Introduced with VNA Rev:

IPowerSensorCalFactorSegment

9.0