Read-only |
About Segment SweepAbout PMAR |
Description |
Returns the number of the current segment, PowerSensorCalFactorSegment or PowerLossSegment object. |
VB Syntax |
seg.SegmentNumber |
Variable |
(Type) - Description |
seg |
Any of the following objects: A Segment (Object) A PowerSensorCalFactorSegment (Object) A PowerSensorCalFactorSegmentPMAR Object (Object) A PowerLossSegment (Object) A PowerLossSegmentPMAR (Object) |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
segNum = seg.SegmentNumber 'returns the segment number -Read |
C++ Syntax |
HRESULT get_SegmentNumber(long *pVal) |
Interface |
ISegment IPowerLossSegment |