Write/Read |
About Swept IMD |
Description |
Sets and returns the offset that is applied to CSO measurements. Valid only with measurement parameters: CSO2Lo and CSO2Hi. |
VB Syntax |
imd.CSOOffset = value |
Variable |
(Type) - Description |
imd |
A SweptIMD Object |
value |
(Double) Offset value in dBm. |
Return Type |
Double |
Default |
0 |
Examples |
imd.CSOOffset = 2 'Write |
value = imd.CSOOffset 'Read |
|
C++ Syntax |
HRESULT get_CSOOffset(double *pVal) |
Interface |
ISweptIMD |