Write/Read | 
About Swept IMD | 
Description | 
 Sets and returns the offset that is applied to CTB measurements. Valid only with measurement parameters: CTB, CTBLo, CTBHi, CTBE, CTBELo, and CTBEHi.  | 
VB Syntax | 
 imd.CTBOffset = value  | 
Variable | 
(Type) - Description | 
| 
 imd  | 
 A SweptIMD Object  | 
| 
 value  | 
 (Double) Offset value in dBm.  | 
Return Type | 
 Double  | 
Default | 
 0  | 
Examples | 
 imd.CTBOffset = 2 'Write  | 
| 
 value = imd.CTBOffset 'Read  | 
|
C++ Syntax | 
 HRESULT get_CTBOffset(double *pVal)  | 
Interface | 
 ISweptIMD  |