Write/Read
About SweptIMDCal

CalibrationFrequencies Property


Description

Sets and returns the whether to perform the source power cal at the center frequencies midway between the main tones, or at all main tone frequencies.

 VB Syntax

imd.CalibrationFrequencies = value

Variable

(Type) - Description

imd

A SweptIMDCal (object)

value

(Enum as NAIMDCalibrationFrequencies)  Choose from:

0 - naIMDCenterFrequencies -Perform source power calibration at only the center frequencies midway between the main tones.

1 - naIMDALLFrequencies - Perform source power calibration at all main tone frequencies.

Return Type

Enum

Default

0 - naIMDCenterFrequencies

Examples

imd.CalibrationFrequencies = naIMDALLFrequencies 'Write

calFreq = imd.CalibrationFrequencies 'Read

C++ Syntax

HRESULT get_CalibrationFrequencies(tagNAIMDCalibrationFrequencies * Val)

HRESULT put_CalibrationFrequencies(tagNAIMDCalibrationFrequencies newVal)

Interface

ISweptIMD