SweptIMDCal Object


Description

Sets properties that are unique to a Swept IMD Cal (opt S93087A/B).

Use the Guided Calibration commands for the remaining commands to perform a Swept IMD Cal

Accessing the SweptIMDCal object

Dim app as AgilentPNA835x.Application

Set IMDcal = pna.GetCalmanager.CreateCustomCalEx(channelNum)

Set IMDCalExtension = IMDcal.CustomCalConfiguration

IMDCalExtension.PowerLevel = 5

See Also:

Method

Interface

See History

Description

None

 

 

Property

Interface

Description

CalibrationFrequencies

ISweptIMDCal

Perform the source power cal at the center frequencies or at all main tone frequencies.

CalMethod

ISweptIMDCal

Sets the method by which the match-correction portion of an IMD cal is performed

EnableLOPowerCal

ISweptIMDCal2

Enable or disable an LO power cal with an IMDx calibration.

Include2ndOrderProduct

ISweptIMDCal

Include the second order products in the calibration.

MaxProduct

ISweptIMDCal

Sets and returns the maximum intermod product frequencies to be calibrated.

PowerLevel

ISweptIMDCal

Set and read the power level of the source power cal.

PowerSensorCalKitType

ISweptIMDCal

Set and read the cal kit to be used for port 1 adapter compensation.

PowerSensorConnectorType

ISweptIMDCal

Superseded  Use GuidedCal.PowerSensorConnectorType

 

ISweptIMD History

Interface

Introduced with VNA Rev:

ISweptIMDCal

8.33

ISweptIMDCal2

8.55