Write/Read |
About Frequency |
Description |
Sets or returns the center frequency of the channel See the Measurement2 Interface to learn how this method differs from meas.Center. |
VB Syntax |
object.centerFrequency = value |
Variable |
(Type) - Description |
object |
A Channel (object) or A Segment (object) |
value |
(double) - Center frequency in Hertz. Choose any number between the minimum and maximum frequencies of the analyzer. |
Return Type |
Double |
Default |
Center of the frequency range |
Examples |
chan.centerFrequency = 4.5e9 'sets the center frequency of a linear sweep for the channel object -Write |
centfreq = chan.centerFrequency 'Read |
|
C++ Syntax |
HRESULT get_CenterFrequency(double *pVal) |
Interface |
IChannel ISegment |