Write/Read |
About Swept IMD |
Description |
Sets and returns the CSO Power for POWER normalization mode. Valid only with measurement parameters: CSO2Lo and CSO2Hi and for Normalization Modes dBm and dBmV. |
VB Syntax |
imd.CompositeNormalizedCSOPower = value |
Variable |
(Type) - Description |
imd |
A SweptIMD Object |
value |
(Double) Power level. The units are determined by CompositeNormalizationMode Property, which must be set first. |
Return Type |
Double |
Default |
0 |
Examples |
imd.CompositeNormalizedCSOPower = -5 'Write |
value = imd.CompositeNormalizedCSOPower 'Read |
|
C++ Syntax |
HRESULT get_CompositeNormalizedCSOPower(double *pVal) |
Interface |
ISweptIMD |