Write/Read |
About Swept IMD |
Description |
Sets and returns the starting main tone separation for sweep type= naIMDDeltaFrequencySweep |
VB Syntax |
imd.DeltaFrequencyStart = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMD Object |
|
value |
(Double) - Starting tone separation between F1 and F2 in Hz. Both F1 and F2 tones MUST be within the frequency range of the VNA where: F1 (start) = imd.FrequencyCenter – imd.DeltaFrequencyStart / 2 F2 (start) = imd.FrequencyCenter + imd.DeltaFrequencyStart / 2 |
Return Type |
Double |
Default |
1 MHz |
Examples |
imd.DeltaFrequencyStart = 5e6 'Write |
|
value = imd.DeltaFrequencyStart 'Read |
|
C++ Syntax |
HRESULT get_DeltaFrequencyStart(double *pVal)) |
Interface |
ISweptIMD |