Write/Read |
About Swept IMD |
Description |
Sets and returns the stop spacing of the main tones. Use with sweep type= naIMDDeltaFrequencySweep |
VB Syntax |
imd.DeltaFrequencyStop = value |
Variable |
(Type) - Description |
|
imd |
A SweptIMD Object |
|
value |
(Double) - Stopping tone separation between F1 and F2 in Hz. Both F1 and F2 tones MUST be within the frequency range of the VNA where: F1 (stop) = imd.FrequencyCenter – imd.DeltaFrequencyStop / 2 F2 (stop) = imd.FrequencyCenter + imd.DeltaFrequencyStop / 2 |
Return Type |
Double |
Default |
10 MHz |
Examples |
imd.DeltaFrequencyStop = 20e6 'Write |
|
value = imd.DeltaFrequencyStop 'Read |
|
C++ Syntax |
HRESULT get_DeltaFrequencyStop(double *pVal)) |
Interface |
ISweptIMD |