Read-Write
About FOM

Divisor Property


Description

Sets and returns the Divisor value to be used when coupling this range to the primary range.

This setting is valid only if the specified range is coupled to the primary range.

 VB Syntax

FOMRange.Divisor = value

Variable

(Type) - Description

object

An FOMRange (object)

value

(Double) - Divisor value.-(Unitless)

Return Type

Double

Default

0

Examples

fomRange.Divisor = .5 'Write

Div = fomRange.Divisor 'Read

C++ Syntax

HRESULT get_Divisor(double  *pVal)
HRESULT put_Divisor(double *pVal)

Interface

IFOMRange