| Write/Read | About Frequency Offset | 
| Description | This method is replaced by properties on the FOMRange Object. Specifies (along with FrequencyOffsetMultiplier) the value to multiply by the stimulus. See other Frequency Offset properties | 
| VB Syntax | object.FrequencyOffsetDivisor = value | 
| Variable | (Type) - Description | 
| object | Channel (object) or CalSet (object) - Read-only property | 
| value | (Double) - Divisor value. Range is 1 to 1000 | 
| Return Type | Double | 
| Default | 1 | 
| Examples | chan.FrequencyOffsetDivisor = 2 'Write | 
| fOffsetDiv = chan.FrequencyOffsetDivisor 'Read | |
| C++ Syntax | HRESULT get_FrequencyOffsetDivisor(double*pval) HRESULT put_FrequencyOffsetDivisor(double newVal) | 
| Interface | IChannel2 |CalSet3 |