Write/Read |
About Frequency Offset |
Description |
This method is replaced by properties on the FOMRange Object. Specifies an absolute offset frequency in Hz. For mixer measurements, this would be the LO frequency. See other Frequency Offset properties. |
VB Syntax |
object.FrequencyOffsetFrequency = value |
Variable |
(Type) - Description |
object |
Channel (object) or CalSet (object) - Read-only property |
value |
(Double) - Offset value. Range is +/- 1000 GHz. (Offsets can be positive or negative.) |
Return Type |
Double |
Default |
0 Hz |
Examples |
chan.FrequencyOffsetFrequency = 2 'Write |
fOffsetFreq = chan.FrequencyOffsetFrequency 'Read |
|
C++ Syntax |
HRESULT get_FrequencyOffsetFrequency(double*pval) |
Interface |
IChannel2 |CalSet3 |