Write/Read
About Mixer Configuration

IFDenominator Property


Description

Sets or returns the denominator value of the IF Fractional Multiplier.

Only applies to 2 stage mixers.

If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface.

 VB Syntax

conv.IFDenominator = value

Variable

(Type) - Description

conv

A  Converter (object)

value

(long) IF Denominator value.

Return Type

Long

Default

1

Examples

Print mixer.IFDenominator 'prints the value of the IFDenominator

C++ Syntax

HRESULT get_IFDenominator(long *pVal)

HRESULT put_IFDenominator(long newVal)

Interface

IConverter4