Write/Read
About Mixer Configuration

IFNumerator Property


Description

Sets or returns the numerator value of the IF Fractional Multiplier.

Only applies to 2 stage mixers.

If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface.

 VB Syntax

conv.IFNumerator = value

Variable

(Type) - Description

conv

A Converter (object)

value

(Long) IF Numerator value.

Return Type

long

Default

1

Examples

Print mixer.IFNumerator 'prints the value of the IFNumerator

C++ Syntax

HRESULT get_IFNumerator(long *pVal)

HRESULT put_IFNumerator(long newVal)

Interface

IConverter4