Write/Read |
About Mixer Configuration |
Description |
Sets or returns the stop frequency value of the mixer IF frequency. Only applies to 2 stage mixers. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. |
VB Syntax |
mixer.IFStopFrequency = value |
Variable |
(Type) - Description |
mixer |
A Converter (object) |
value |
(double) - IF stop frequency in Hertz. |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Print mixer.IFStopFrequency 'prints the value of the IFStopFrequency |
C++ Syntax |
HRESULT get_IFStopFrequency(double *pVal) HRESULT put_IFStopFrequency(double newVal) |
Interface |
IMixer |