Write/Read |
About Mixer Configuration |
Description |
Sets or returns the mixer fixed Input frequency value. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. |
VB Syntax |
obj.InputFixedFrequency = value |
Variable |
(Type) - Description |
obj |
A Mixer Interface pointer to the Measurement (object) Or |
value |
(double) - Input Fixed Frequency in Hertz. |
Return Type |
Double |
Default |
Not Applicable |
Examples |
mixer.InputFixedFrequency = 1e9 |
C++ Syntax |
HRESULT get_InputFixedFrequency(double *pVal) HRESULT put_InputFixedFrequency(double newVal) |
Interface |
IMixer6 IConverter |