Write/Read
About Mixer Configuration

LOFixedFrequency Property


Description

Sets or returns the LO frequency value.

If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface.

 VB Syntax

obj.LOFixedFrequency (n) = value

Variable

(Type) - Description

obj

A Mixer Interface pointer to the Measurement (object)

Or

A Converter Object

value

(double) - LO Frequency in Hertz.

n

(Long)  - LO stage number

Choose from 1 or 2

Return Type

Double

Default

0 Hz

Examples

Print mixer.LOFixedFrequency(1) 'prints the value of the first LO fixed frequency

C++ Syntax

HRESULT get_LOFixedFrequency(double *pVal)

HRESULT put_LOFixedFrequency(double newVal)

Interface

IMixer

IConverter