| Write/Read | About Mixer Configuration | 
| Description | Sets or returns the LO stop frequency value. This command can only be used with SMC (not VMC) measurements. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. | 
| VB Syntax | obj.LOStopFrequency (n) = value | 
| Variable | (Type) - Description | 
| obj | A Mixer Interface pointer to the Measurement (object) Or | 
| value | (double) - LO Stop Frequency in Hertz. | 
| n | (Long) - LO stage number Choose from 1 or 2 | 
| Return Type | Double | 
| Default | Not Applicable | 
| Examples | Print mixer.LOStopFrequency(1) 'prints the value of the first LO stop frequency | 
| C++ Syntax | HRESULT get_LOStopFrequency(long id, double *pVal) HRESULT put_LOStopFrequency(long id,double newVal) | 
| Interface | IMixer3 IConverter |