Read-only
About Embedded LO

MarkerAnnotation Property


Description

Returns the Y-axis marker value from the specified tuning sweep. Use IsMarkerOn to confirm if a marker was used for the tuning sweep.

 VB Syntax

value = embedLODiag.MarkerAnnotation (n)

Variable

(Type) - Description

value

(String) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

n

(Long) Tuning sweep number. Use NumberOfSweeps to find the number of sweeps taken.

Default

Not Applicable

Examples

data= embedLO.MarkerAnnotation 3 'read

C++ Syntax

HRESULT MarkerAnnotation(long sweep, BSTR* annotation);

Interface

IEmbededLODiagnostic