Read-Write
About FOM

Multiplier Property


Description

Sets and returns the multiplier value to be used when coupling this range to the primary range. Learn more about multiplier value.

This setting is valid only if this range is coupled to the primary range.

 VB Syntax

FOMRange.Multiplier = value

Variable

(Type) - Description

object

An FOMRange (object)

value

(Double) - Multiplier value.-(Unitless)

Return Type

Double

Default

1

Examples

fomRange.Multiplier = 2 'Write

Mult = fomRange.Multiplier 'Read

C++ Syntax

HRESULT get_Multiplier(double  *pVal)
HRESULT put_Multiplier(double pVal)

Interface

IFOMRange