| Write/Read | About Number of Points | 
| Description | Sets or returns the Number of Points of the channel. Sets or returns the Number of Points of the segment. See Also
 | 
| VB Syntax | object.NumberOfPoints = value | 
| Variable | (Type) - Description | 
| object | Channel (object) or CalSet (object) - Read-only property | 
| value | (long) - Number of Points. For channel, choose any number from 1 to the VNA max number of points. For segment, the total number of points in all segments cannot exceed the VNA maximum. A segment can have as few as 1 point. | 
| Return Type | Long Integer | 
| Default | 201 for channel 21 for segment | 
| Examples | chan.NumberOfPoints = 201 'sets the number of points for all measurements in the channel. -Write | 
| numofpts = chan.NumberOfPoints 'Read | |
| C++ Syntax | HRESULT get_NumberOfPoints(long *pVal) | 
| Interface | IChannel |CalSet3 |