Write/Read
About Mixer Configuration

OutputFixedFrequency Property


Description

Sets or returns the mixer output fixed frequency value.

If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface.

 VB Syntax

obj.OutputFixedFrequency = value

Variable

(Type) - Description

obj

A Mixer Interface pointer to the Measurement (object)

Or

A Converter Object

value

(double) - Output Fixed Frequency in Hertz.

Return Type

Double

Default

Not Applicable

Examples

Print mixer.OutputFixedFrequency 'prints the output fixed frequency value of the mixer.

C++ Syntax

HRESULT get_OutputFixedFrequency(double *pVal)

HRESULT put_OutputFixedFrequency(double newVal)

Interface

IMixer3

IConverter