Write/Read |
About Mixer Configuration |
Description |
Specify whether to select the sum (High) or difference (Low) products.
Use IFSideband_Property when two LOs are used to determine the IF1 frequency. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. Note: There is also an OutputSideband_Property on the Converter Object. |
VB Syntax |
mixer.OutputSideband = value |
Variable |
(Type) - Description |
mixer |
A Mixer (object) |
value |
(FCASideBand) - Choose from: 0 - LOW Minus (-) on the Mixer setup dialog 1 - HIGH Plus (+) on the Mixer setup dialog |
Return Type |
Enum as FCASideBand |
Default |
LOW |
Examples |
Print mixer.OutputSideband 'prints the value of the OutputSideband |
C++ Syntax |
HRESULT get_OutputSideband(FCASideBand *pVal) HRESULT put_OutputSideband(FCASideBand newVal) |
Interface |
IMixer |