| Write/Read | About Mixer Configuration | 
| Description | Sets or returns the mixer output start frequency. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. | 
| VB Syntax | obj.OutputStartFrequency = value | 
| Variable | (Type) - Description | 
| obj | A Mixer Interface pointer to the Measurement (object) Or | 
| value | (double) - Output Start Frequency in Hertz. | 
| Return Type | Double | 
| Default | Not Applicable | 
| Examples | Print mixer.OutputStartFrequency 'prints the value of the OutputStartFrequency | 
| C++ Syntax | HRESULT get_OutputStartFrequency(double *pVal) HRESULT put_OutputStartFrequency(double newVal) | 
| Interface | IMixer IConverter |