Write/Read
About Fixturing

PortArbzImag Property


Description

Sets and returns the Imaginary portion of the impedance value for the specified single-ended port. Use PortArbzReal to set the real value. Or use PortArbzZ0 to set both values together.

 VB Syntax

fixture.PortArbzImag(portNum) = value

Variable

(Type) - Description

fixture

A Fixturing (object)

portNum

(Integer)  Single-ended port number to receive impedance value.

value

(Double) Real Impedance value. Choose a value between -1E18 and 1E18

Return Type

Double

Default

0

Examples

fixture.PortArbzImag(2) = 75 'Write

value = fixture.PortArbzImag(1) 'Read

C++ Syntax

HRESULT get_PortArbzImag( short portNum, double *pVal)
HRESULT put_PortArbzImag( short portNum, double newVal)

Interface

IFixturing3