Write / Read
About Port Extensions

PortWGCutoffFreqProperty


Description

Sets and returns the cuttoff (minimum) frequency of the added waveguide fixture or transmission line.

 VB Syntax

fixture.PortWGCutoffFreq(port)= value

Variable

(Type) - Description

fixture

A Fixturing Object

port

(Integer) Port Number for which media type is being set.

value

(Double) Cutoff frequency in Hz.

This value is ignored when PortMedium Property is set to COAX for the same port.

Return Type

Double

Default

System Media Cutoff Frequency

Examples

fixture.PortWGCutoffFreq(2)= 1e9 'Write

value = fixture.PortWGCutoffFreq(2) 'Read

C++ Syntax

HRESULT get_PortWGCutoffFreq(short portNum, double *pVal);

HRESULT put_PortWGCutoffFreq(short portNum, double newVal);

Interface

IFixturing4