Read-only
About Cal All

SParameterCalPorts Property


Description

Read the final list of ports that will be fully calibrated by Calibrate All Channels.  For the returned list of ports, specify connectors and cal kits for the calibration using the GuidedCal commands.

Ports to received ONLY a power cal (such as mixer LO ports) will NOT be on the returned list.

For each channel, specify the ports to be calibrated using CalibrationPorts Property

 VB Syntax

ports = calAll.SParameterCalPorts

Variable

(Type) - Description

ports

(Variant Array) Ports to be calibrated.

calAll

A CalibrateAllChannels (object)

Return Type

Variant Array

Default

Not Applicable

Examples

ports = calAll.SParameterCalPorts 'returns the ports to be cal'd

C++ Syntax

HRESULT SParameterCalPorts([out,retval] VARIANT* calports);

Interface

ICalibrateAllChannels