Write/Read
About Mixer/Converter Settings

SegmentStartFrequency Property


Description

Set and read the start frequency for the mixer segment. The specified SegmentRangeMode must be set to Swept.

Send Apply before sending a query (read). Learn more.

 VB Syntax

conv.SegmentStartFrequency(index,range) = value

Variable

(Type) - Description

conv

A Converter Object

index

(Long integer) Segment for which start frequency is being set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer.

range

(Enum as ConverterFrequencyRange) Range for which start frequency is being set. Choose from:

0 - naInputFrequencies - set input frequency

1 - naOutputFrequencies - set output frequency

2 - naLO1Frequencies - set LO1 frequency

3 - naLO2Frequencies - set LO2 frequency

4 - naIFFrequencies - set IF frequency

value

(Double) Start frequency. Choose a value within the frequency range of the VNA.

Return Type

Double

Default

Start frequency of the VNA

Examples

mxr.SegmentStartFrequency(1,0)=1e9 'sets the input start frequency to 1 GHz

See example program

C++ Syntax

HRESULT get_SegmentStartFrequency(long index, tagConverterFrequencyRange range, double *value);

HRESULT put_SegmentStartFrequency(long index, tagConverterFrequencyRange value, double value);

Interface

IConverter5