| Write/Read | About IM Spectrum | 
| Description | When an IMD channel exists, allows the IM Spectrum frequency and power setting to track (couple with) the IMD channel settings. Use TrackingChannel to set the channel number to track. | 
| VB Syntax | ims.TrackingEnable = value | 
| Variable | (Type) - Description | 
| ims | An IMSpectrum Object | 
| value | (Boolean) Tracking state. Choose from: True - IM Spectrum frequency and power settings track the IMD channel settings. False - IM Spectrum frequency and power settings are specified in the IMS channel. | 
| Return Type | Boolean | 
| Default | False | 
| Examples | ims.TrackingEnable = True 'Write | 
| value = ims.TrackingEnable 'Read | |
| C++ Syntax | HRESULT get_TrackingEnable(VARIANT_BOOL* bValue) | 
| Interface | IIMSpectrum |