Controls the IM Spectrum settings.
| Dim app as AgilentPNA835x.Application app.CreateCustomMeasurementEx(1, "IMSpectrum", "Output", 1) Dim IMSpec Set IMSpec = app.ActiveChannel.CustomChannelConfiguration | 
Example Program Create and Cal a IM Spectrum Measurement
| Method | InterfaceSee History | Description | 
|---|---|---|
| IIMSpectrum | Sets limited port mapping | |
| Property | Interface | Description | 
| IIMSpectrum | ON | OFF state of power coupling for F1 and F2. | |
| IIMSpectrum | Read input port map | |
| IIMSpectrum | Read output port map | |
| IIMSpectrum | Fixed tone spacing value. | |
| IIMSpectrum2 | Superseded with LevelingMethod Set Equal Tone Power state. | |
| IIMSpectrum | Frequency of the F1 tone. | |
| IIMSpectrum | Frequency of the F2 tone. | |
| IIMSpectrum | Center frequency of the main tones. | |
| IIMSpectrum3 | Set tone power leveling mode | |
| IIMSpectrum | Resolution Bandwidth for the measurement. | |
| IIMSpectrum | Receiver Center frequency | |
| IIMSpectrum | Receiver frequency span. | |
| IIMSpectrum | Receiver Start frequency. | |
| IIMSpectrum | Receiver Stop frequency. | |
| IIMSpectrum2 | Superseded with LevelingMethod Set power at DUT input or Output | |
| IIMSpectrum | IMD channel number to which the IM Spectrum channel is coupled. | |
| IIMSpectrum | Enables tracking with an IMD channel. | |
| IIMSpectrum | Step sweep mode for the IM Spectrum channel. | |
| IIMSpectrum | IMD data point number at which the IM spectrum measurement occurs. | |
| IIMSpectrum | IM product to view when SweepType = NTH is specified. | |
| IIMSpectrum | Type of sweep for an IMSpectrum measurement. | |
| IIMSpectrum | Power level of the Main Tones | 
| Interface | Introduced with VNA Rev: | 
| IIMSpectrum | 8.35 | 
| IIMSpectrum2 | 9.40 |