| Write/Read | About IM Spectrum Tracking | 
| Description | Sets and returns the step sweep mode for the IM Spectrum channel. | 
| VB Syntax | ims.TrackingManualStepEnable = value | 
| Variable | (Type) - Description | 
| ims | An IMSpectrum Object | 
| value | (Boolean) Choose from: False - Automatic Step True - Manual Step | 
| Return Type | Boolean | 
| Default | False - Automatic Step | 
| Examples | ims.TrackingManualStepEnable = True 'Write | 
| value = ims.TrackingManualStepEnable 'Read | |
| C++ Syntax | HRESULT get_TrackingManualStepEnable(VARIANT BOOL *bVal) | 
| Interface | IIMSpectrum |