Write/Read |
About Trigger Mode |
Description |
These settings determine what EACH signal will trigger. Note: Setting Point and EverySweep mode forces Trigger.Scope = naChannelTrigger. |
VB Syntax |
chan.TriggerMode = value |
Variable |
(Type) - Description |
chan |
A Channel (object) |
value |
(enum NATriggerMode) - Choose from: 0 - naTriggerModePoint - Each Manual or External trigger signal causes one data point to be measured. 1 - naTriggerModeMeasurement (superseded - still works but replaced with a more descriptive enum) 1 - naTriggerModeChannel - Each trigger signal causes ALL traces in that channel to be swept. 2 - naTriggerModeEverySweep - Each Manual or External trigger signal causes ALL traces that share a source port to be swept. 3 - naTriggerModeTrace - Allowed ONLY when PointSweepState is enabled. Each trigger signal causes two identical measurements to be triggered separately - one trigger signal is required for each measurement. Other trigger mode settings cause two identical parameters to be measured simultaneously. |
Return Type |
Long Integer |
Default |
1 - naTriggerModeChannel |
Examples |
chan.TriggerMode = naTriggerModePoint 'Write |
trigtyp = chan.TriggerMode 'Read |
|
C++ Syntax |
HRESULT get_TriggerMode (tagNATriggerMode *pMode) |
Interface |
IChannel |