| Write/Read | About Path Configurator | 
| Description | Write or read a value (setting) for the current element. This command is used to set both RF and IF Path Configuration. | 
| VB Syntax | pathElement.Value = value | 
| Variable | (Type) - Description | 
| pathElement | A PathElement (object) | 
| value | (String) Value for the element. Use pathElement.Values to return a list of valid settings for this element. | 
| Return Type | String | 
| Default | Not Applicable | 
| Examples | See Examples: | 
| C++ Syntax | HRESULT get_Value( BSTR* pValue ); HRESULT put_Value( BSTR value ); | 
| Interface | IPathElement |